8/6/2008 3:59 PM | |
Joined: 10/19/2005 Last visit: 11/30/2020 Posts: 1611 Rating: (121) |
Hi, normaly when you create a new project, then you have the follwing data (Sample!) -> PROJECT_1.hmi -> PROJECT_1_log.LDF This two data are very importent. Maybe you have only the "PROJECT_1.hmi" file. So you get your message. (In some cases it could be work without the "PROJECT_1_log.LDF", but normally you need this data) More Info you can find under this link -> http://support.automation.siemens.com/WW/view/en/21896449 regards |
8/8/2008 10:33 AM | |
Posts: 29 Rating: (1) |
Maybe... try to check the edit date in the Windows Explorer Window If dates differ try to get the corresponding file with same date... ? greets HelixX²³ |
2/12/2015 1:26 PM | |
Posts: 2 Rating: (0) |
Hi, I also have the same problem. Even with the archive file. It was created in WinCC 2005/6 and I give me this message when opening it. Regards
|
Follow us on