1/25/2016 1:56 PM | |
Joined: 8/19/2012 Last visit: 5/22/2024 Posts: 125 Rating:
|
dears i have a problem with LOGO !TD please advice me to solve this problem as mention below : problem:- I did a project via logo software but during download to LOGO i found error .IF i removed message text and download the project to LOGO it is ok. but when i downloaded it with message text i get a problem. So i send also the project LOGO .if any one repair it . so pleas help me. Type of logo LOGO!230RC AS/DC 115 240V .6ED1 052-1FB00-0BA4 best regards ------------------------------------------------------------------------------------------ AttachmentCircuit Diagram1ok last one oregenal.rar (160 Downloads) |
Last edited by: Min_Moderator at: 1/25/2016 3:44:14 PMNew subject after splitting |
|
1/27/2016 1:29 PM | |
Joined: 8/5/2015 Last visit: 9/20/2021 Posts: 120 Rating:
|
H |
Last edited by: kormotech at: 1/27/2016 1:48:10 PM |
|
1/27/2016 1:30 PM | |
Joined: 8/5/2015 Last visit: 9/20/2021 Posts: 120 Rating:
|
A |
Last edited by: kormotech at: 1/27/2016 1:48:38 PM |
|
Follow us on