1/19/2017 8:47 PM | |
Posts: 1 Rating: (0) |
I know I am hijacking an extremely old post here but I could not post a question any other way. The pulse output for this flowmeter, does it have to be a powered loop at all times?? I have a data logger connected which with PGEN set to 1 pulse per litre gives me a matching flow rate with the flowmeter. Unfortunately as the flow is between 50 and 100l/s and the logger in question can handle max 36hz it is not recording anything other than a flatline 36.4l/s. When changing PGEN to 0.1 or 0.01 this fails to show any flow instantaneously within the logger and also records a flatline zero. Any advice I am struggling to get my head round why it works at 1 litre per pulse but not at any other setting. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 1/20/2017 12:56:58 PMNew subject after splitting |
|
Follow us on