8/30/2017 11:55 AM | |
Posts: 2 Rating:
|
Hi there, I managed to access my LOGO 0ba8 both web server and smart phone connections via LAN (Wifi connection), but the problem is the internet connection. Firstly, I tried to connect by using Dion64 description. But it was not suitable as I use LOGO 8 and LOGO! Soft Comfort 8.1. What's more, the router had a different setting that I've attached here. The problems that I need to solve are here: - What is the exact setting of my router? such as Application, Start Port number, End port number, and so on. - I made a DDNS URL by using Noiop. Is there any need for using this method to connect my LOGO? If so, how can I set my router and software? - what is the gateway in LOGO network setting? Thank you! ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 8/30/2017 1:33:45 PMNew subject after splitting Last edited by: The Helping Hand at: 9/7/2017 2:07:18 PM |
|
This contribution was helpful to
1 thankful Users |
2/17/2020 6:58 AM | |
Posts: 4 Rating:
|
have you managed? I have the exact same questions :) |
Follow us on