9/5/2017 4:38 AM | |
Posts: 1 Rating:
|
Hello All, I am new to Siemens step 7 and need all the help I can get. I have an analog 4-20 mA signal from a level transmitter (I have 6ES7 331-7RD00-0AB0 Input module). Please advise me what is the input signal type (Real, Word , Integer or some thing like MD). If it is MD or any thing else, please tell me how I can configure it. Thanks ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 9/5/2017 7:37:37 AMNew subject after splitting |
|
9/5/2017 7:28 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating:
|
hi, have a look in this manual, chapter 5: SIMATIC S7-300 S7-300 Module data normally it is an integer with a value from 0-27648 for 0-100% or from -27647 to 27648 for -100% to 100%. Devices with Measurement for temperature are showing the temperature in 1/10 or 1/100 degree. hope this helps, regards, |
FCK WAR! |
|
Follow us on