11/23/2010 1:27 AM | |
Joined: 7/2/2008 Last visit: 7/2/2024 Posts: 928 Rating: (306)
|
Dear Clodoaldopuc, I recommend toread the following, How can you obtain an overview of the memory concept of SIMATIC S7-300 CPUs and C7 devices? How can I get an overview of the S7-400 memory concept? In S7-300, neither the load memory nor the work memory is expandable. For example check the specs. of S7315-2DP In S7-400, the integrated load memory of the CPU can be expanded by the memory card (Check the specs. of 414-3). Normally, you should care more about the work memory capacity not the load memory. You can backup your project on the memory card if you have enough space. This is always the case in S7-300 while in S7-400 you need either RAM memory card with backup batteries ora FLASH memory card. Yes, all at the same time. Best regards, H-H |
Last edited by: O_Moderator at: 11/23/2010 7:40 AMlinks edited |
|
11/23/2010 10:06 AM | |
Joined: 7/2/2008 Last visit: 7/2/2024 Posts: 928 Rating: (306)
|
Dear Wizard, Thanks for your contribution. I believe I didn't use the right words in my previous post. I said the load memory is not expandable since it's not located in the CPUto be expanded.
Best regards, H-H |
This contribution was helpful to1 thankful Users |
4/24/2014 8:12 AM | |
Posts: 340 Rating: (6) |
new question is splittet to Work memmory full, S7-314C-2ptp, What can I do?. |
7/27/2014 2:42 PM | |
Posts: 6 Rating: (0) |
hi i have a question please answer me .. tanx : until,, there is not backup battery , how run the control program ?? |
Follow us on