2/27/2012 12:32 PM | |
Joined: 9/28/2005 Last visit: 11/5/2024 Posts: 2957 Rating: (242)
|
look here: Discontinuation: SIMATIC TP 270, OP 270 and MP 270TP270 10" is replaced by MP277 8" (6AV6643-0CB01-1AX1), so maybe its better to go for it ? First I thought it will be resolution issue, but I've checked all panel and all have 640x480 resolution so in any case your pictures will not be corrupted by resolution conversion. So I think you can go for any of those two panels. |
Last edited by: Darius at: 2/27/2012 12:43 PMBest regards, |
|
2/27/2012 12:38 PM | |
Joined: 4/29/2010 Last visit: 8/12/2024 Posts: 1557 Rating: (161)
|
Hi, the conversion itself doesn´t work without any changes in your configuration (caused f. e. by the settings of the area pointers wich are different at WinCC flexible). If you want to check what have to be done if you convert this project to flexible (in a MP277) i advice you to take a look at the migration manual (chapter 3): WinCC flexible migration manual For the replacement of a MP270, the MP277 is the best choice. The MP277 is the successor type of the MP270 and full compatible. For more information take a look at the phased-out actual information: Phased-out Products: SIMATIC TP 270, OP 270 and MP 270 best regards |
2/27/2012 2:41 PM | |
Joined: 8/18/2009 Last visit: 6/17/2024 Posts: 548 Rating: (33) |
|
Rajkiran Patil |
|
2/28/2012 8:26 AM | |
Joined: 9/28/2005 Last visit: 11/5/2024 Posts: 2957 Rating: (242)
|
No, that's not true. Look here: Discontinuation: SIMATIC TP 270, OP 270 and MP 270 Actually it can't be a replacement as TP270 was 10" and 640x480 resolution and the only one version of TP277 is 6" 320x240 resolution. So it just can't be a replacement. |
Last edited by: Darius at: 2/28/2012 8:40 AMBest regards, |
|
Follow us on