3/12/2013 12:43 PM | |
Joined: 9/27/2006 Last visit: 4/19/2024 Posts: 12256 Rating: (2664) |
Hello Fahud; Most of your questions will find their answers in the following link from the Siemens Insdustry Mall: https://eb.automation.siemens.com/mall/en/WW/Catalog/Products/10020787
SITRANS F M Verificator (MAG 5000 and 6000) The SITRANS F M Verificator is an external tool designed for MAG 5000 and MAG 6000 with MAG 1100, MAG 1100 F, MAG 3100, MAG 3100 P or MAG 5100 W sensors to verify the entire product, the installation and the application. The goal is to improve operation, reduce downtime and maintain measurement accuracy as long as possible. The SITRANS F M Verificator is highly advanced and carries out the complex verification and performance check of the entire flowmeter system, according to unique SIEMENS patented principles. The whole verification test is automated and easy to operate so there is no opportunity for human error or influence. The system is traceable to international standards and tested by WRc (Water Research Council). Certificate The test certificate generated by a PC contains:
Note: |
Follow us on