12/26/2005 7:18 PM | |
Joined: 9/23/2005 Last visit: 3/11/2024 Posts: 4325 Rating: (1416) |
Hi, I know two alternatives: 1 – Use M7 (but is not more available, see Update http://support.automation.siemens.com/WW/view/en/14044569 ) 2 – Use a PC + C program + WinAC (only as input / output interface). |
Denilson Pegaia |
|
1/10/2006 1:09 PM | |
Joined: 8/31/2005 Last visit: 10/23/2023 Posts: 217 Rating: (40) |
Hi DEBU! For programming an S7 controller you can't use C or C++ directly. You can use the programming language S7-SCL, which is an high-level programming language for S7 controllers (similar to PASCAL). S7-SCL can be used for all nearly S7 controllers. The other way (as Pagaia mentioned) is to use WinAC (a software S7 controller, which is running on a PC) together with WinAC ODK. Have a look at the A&D Mall (https://mall.automation.siemens.com/) for a detailled description of WinAC ODK. Here is an example for using the WinAC ODK: Linking Windows Applications to WinAC RTX with WinAC ODK |
Greetings, Chris |
|
Follow us on