8/11/2009 12:18 PM | |
Joined: 9/6/2007 Last visit: 9/13/2024 Posts: 81 Rating: (1) |
Dear Sirs: I created a CCX program by WinAC ODK V4.2. The environment is VC++ 6.0. I just use a windows dll . Not RTDLL. My purpose is to read a csv file and find a value . Then I write the index of this value to S7 memory.(MW500) But the read csv function doesn't work and the write value to S7 memory works in the DLL. I also identify my source code of read csv function. I create a Win32 console application (*.exe) and put the same code of read csv function. The application can work. So, I don't know why the DLL can't work but the application can work. ps:(a).My test platform: WinAC RTX v4.4.1 in a Panel PC 677. (b).The attached files: One is the CCX program created by ODK4.2. The other is my identified Win32 application of read csv
function. C1.csv is the test file. Tks. Angus. Attachment0811CCX.zip (333 Downloads) |
Follow us on