2/6/2020 7:57 PM | |
Joined: 5/6/2010 Last visit: 3/27/2024 Posts: 1954 Rating: (266) |
Hello, you can't use the NPN-signals directly at your CPU or the FM350. If you need the signals for counting then can you convert the signal from NPN to PNP with a converter e.g. Switching amplifier - DEK-TR/INV - 2964319 from Phoenix Contact. If you need "only" slower inputs then can you use the Digital input module SM 321; DI 64 x DC 24 V, sinking/sourcing; (6ES7321-1BP00-0AA0) regards |
This contribution was helpful to1 thankful Users |
2/9/2020 8:29 PM | |
Posts: 6 Rating: (0) |
Thank you CaOd! You've been very helpful! BR |
2/18/2020 2:02 PM | |
Joined: 8/7/2018 Last visit: 2/27/2024 Posts: 31 Rating: (2) |
I think its OK |
Experience with the process, Steel Making, and logistic systems. |
|
Follow us on