8/24/2011 7:28 AM | |
Posts: 37 Rating: (2) |
if it is on profibus then get GSD for it. if hardwired communication to be done then use FM-350-1 counter module. |
8/24/2011 7:40 AM | |
Joined: 4/14/2010 Last visit: 8/6/2024 Posts: 525 Rating: (11) |
Greeting, Can i connect this encoder to directly with CPU313C..???? |
MS |
|
8/24/2011 7:53 AM | |
Posts: 37 Rating: (2) |
if baumer encoder support PROFIBUS and the vendor is giving gsd file then yes.as 313-c has dp port. |
8/24/2011 8:13 AM | |
Joined: 4/14/2010 Last visit: 8/6/2024 Posts: 525 Rating: (11) |
encoder not profibus i want to connect through wiring with CPU and using SFB48 for encoder is it Possible..??? |
MS |
|
8/24/2011 8:25 AM | |
Posts: 37 Rating: (2) |
But how u will connect to 313-c direct without PROFIBUS? SFB48 can be used when u r using counter module FM |
8/24/2011 8:40 AM | |
Joined: 4/20/2007 Last visit: 9/19/2024 Posts: 727 Rating: (42) |
Hello, This CPU313C does not have a DP interface, but has integrated counters. See this document. From page 167. You will have to use the SFB47 Count block. |
8/24/2011 8:53 AM | |
Posts: 37 Rating: (2) |
|
8/24/2011 8:54 AM | |
Posts: 37 Rating: (2) |
but how to connect encoder without profibus? how t0 wire it? |
Follow us on