4/4/2020 7:57 PM | |
Joined: 8/22/2011 Last visit: 3/27/2024 Posts: 52 Rating: (0) |
Dear Experts, I have cpu 314: 6ES7 314 -6CG03 -0AB0 with MMC 6ES7 952-8LG11-0AA0, suddenly the program is deleted from the cpu, i do memory reset to reload the program from MMC but still has no program on the cpu, i try to download the program from the PG but i have error message : the block/op sys. update is too large, please find screenshot of the error message as attachment, i remove the MMC and do MREST and insert it again i get the same message. could you please help me to know if the MMC is corrupted or the CPU is damaged? Attachmentscreenshot.pdf (148 Downloads) |
Follow us on