7/24/2019 11:39 PM | |
Posts: 20 Rating: (0) |
Hi Scorp, please take a look at my program. Your help is very much appreciated. Matt AttachmentpH.zip (287 Downloads) |
7/25/2019 6:31 AM | |
Joined: 2/22/2008 Last visit: 8/6/2024 Posts: 2698 Rating: (207) |
Try the attached programs, they will work, if the network setup of your program is okay. I only use NAI, NAQ as local memory for Modbus, therefore i also don't need a network diagram. This works fine for years and for me it is recommend, because i mostly use ladder. Compare your version with my 2 versions and try them out with your Modbus server. Regards, Scorp AttachmentHydroponic.zip (316 Downloads) |
This contribution was helpful to1 thankful Users |
7/27/2019 6:54 PM | |
Joined: 2/22/2008 Last visit: 8/6/2024 Posts: 2698 Rating: (207) |
There is no need to be dependent on a S7 license, you can download some alternative communication utilities for different processors for free. Look on the page of Snap7, there is a Step7 Open Source Ethernet Communication Suite for C++, Pascal, Python, Java and also for Arduino (Settimino). I have not used it up to know, but i am planning for the future to write some small utilities with Pascal. With settimino it should be possible to write your own client or server with the S7 protocol. Maybe this is an option for you ? Regards, Scorp |
Follow us on