1/14/2006 1:32 PM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating: (315) |
Hi, Behind this link is some more explanation: http://support.automation.siemens.com/WW/view/en/15261408 You may write back the data from the <Work Memory> to the<Load Memory> with SFC83/84 in a MMC. With that function are the values that you lose now in the MMC (is Load Memory). I have made a FC that also do this for recepy, there are also unlinked datablocks in the Load Memory used so that you for example may use 50 recipes whereby only for 1 receipe the data is in Work Memory. Best regards, Late [:o] |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
Follow us on