11/11/2019 1:46 PM | |
Joined: 4/29/2019 Last visit: 12/3/2023 Posts: 11 Rating: (0) |
Dear all, I have similar problem, could you please help? I use a CPU314 with TP1200 comfort panel. I have to duplicate the HMI with the same hmi project. (We need to control the equippment from two different places) I have already modified the OP communication number from one to two in the cpu communication settings and downloadet. My experience is if I use the same address for both HMI, that either the one or the other HMI is communicating only. But the two at the same time not. The one is communicating which I plug in later. If I use the configuration below the HMI with address 3 does not connect at all. Connection type: MPI (this cpu has only MPI port and only one) CPU Address:2 HMI(1) Address: 1 HMI(2) Address: 3 What else can I do please, I have wasted a lot of time without success! Thank You for your help! ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/11/2019 13:47:26New subject after splitting |
|
Follow us on