6/11/2019 12:39 PM | |
Posts: 9 Rating: (0) |
I it possible to make a program like this in the LOGO! i have made some notes in the zip file, i cant figure out what 'blocks' to use. the light is to be turned on with make contact (I7) this is supposed to turn on the light and start the dynamic light function, (I6) is supposed to stop dynamic light and turn the lights up to max (10V), last the (I5) i supposed to turn off the light. AttachmentDynamic light control.zip (138 Downloads) |
6/11/2019 1:50 PM | |
Posts: 9 Rating: (0) |
the lux range is 30-3000 Lux 30 = 0 V 3000 = 10 V |
This contribution was helpful to1 thankful Users |
6/11/2019 2:36 PM | |
Joined: 12/18/2014 Last visit: 5/13/2024 Posts: 33022 Rating: (0)
|
Here's a possible solution.
AttachmentDynamic light control_V2.zip (147 Downloads) |
This contribution was helpful to1 thankful Users |
6/11/2019 2:56 PM | |
Posts: 9 Rating: (0) |
thanks to you, really helpful, to me at least.. |
This contribution was helpful to1 thankful Users |
6/11/2019 3:00 PM | |
Joined: 12/18/2014 Last visit: 5/13/2024 Posts: 33022 Rating: (0)
|
Hello Jawdragon, you're welcome. Is your problem solved now with this solution? |
Follow us on