10/19/2008 8:55 AM | |
Joined: 9/27/2006 Last visit: 5/11/2024 Posts: 12257 Rating: (2666) |
Hello Radoslaw; Here is some information gathered from the T 200Pro and RF170C manuals: The RF170C is integrated into the ET 200pro hardware configuration by means of an object manager and the GSD file of the interface module. The RF170C can then be configured using HW Config of SIMATIC Manager or another PROFIBUS tool (e.g. operating mode). The object manager or the GSD file can be found on the CD RFID Systems Software & Documentation or on the Internet. Integration into the PROFIBUS master is carried out by means of a GSD file: • SIEM8118.GSD for ET 200pro with IM 154-1 • SIEM8119.GSD for ET 200pro with IM 154-2 High Feature In case you do not have access to the mentionned CD, look in the following link for the ET 200pro gsd file downloads. http://support.automation.siemens.com/WW/view/de/21221197 Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 10/19/2008 8:57 AM |
|
10/19/2008 10:04 AM | |
Joined: 10/18/2008 Last visit: 8/20/2018 Posts: 2 Rating: (0) |
Hello, |
Follow us on