10/25/2017 4:37 PM | |
Posts: 18 Rating: (0) |
Great, it works as I wish !! Thanks !! Now I would like to do the same thing with another entry. I copy / paste the two blocks, I write "1" in V2, 0 in V1, I add a second line in Variable Memory Configuration. Master 2, client, I add a network input, with address VB: 2, but obviously it does not work... it was too easy :) Can your method work only for a only one input? Or there is an other way to configure ? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/26/2017 7:36:51 AMEdited text for better reading. Last edited by: Jen_Moderator at: 10/26/2017 2:40:25 PMNew subject after splitting |
|
10/25/2017 4:57 PM | |
Joined: 12/18/2014 Last visit: 3/29/2024 Posts: 32632 Rating: (4045)
|
In attachment an example.
AttachmentSending_15_bits_from_a_0BA7_to_a_remote_device.zip (176 Downloads) |
This contribution was helpful to1 thankful Users |
10/25/2017 6:48 PM | |
Joined: 12/18/2014 Last visit: 3/29/2024 Posts: 32632 Rating: (4045)
|
I have integrated my UDF blocks into your program (server). Attachment0BA7_master_master_V2.zip (190 Downloads) |
10/25/2017 8:27 PM | |
Joined: 12/18/2014 Last visit: 3/29/2024 Posts: 32632 Rating: (4045)
|
Why? My Support not good? In attachment an exaple for testing and learning. AttachmentSending_15_bits_from_a_0BA7_to_a_0BA7.zip (166 Downloads) |
Last edited by: ixo65 at: 10/25/2017 8:27:25 PMattachment |
|
10/25/2017 10:56 PM | |
Posts: 18 Rating: (0) |
And if I want to communicate client --> serveur is it possible with de same program ? |
Follow us on