9/5/2019 11:42 AM | |
Joined: 4/12/2018 Last visit: 12/19/2023 Posts: 24 Rating: (0) |
Hello, i've downloaded the WP321 "ready to use" projects for both S7-1500 and S7-300 and they seem to work fine in TIA portal 15.1. However, if i copy the WP321 FB to my own projects, TIA portal wants to compile these FB's during download, which fails because they're know-how protected. The same problem exists for the library, it's only available for TIA versions < 15.1, if an older library gets updated there's still this compilation error on the WP321 FB. Is there a TIA portal 15.1 library available by now? regards, ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 09/06/2019 07:52:07New subject after splitting Valar morghulis / Valar dohaeris |
|
9/5/2019 2:13 PM | |
Joined: 1/4/2007 Last visit: 4/18/2024 Posts: 1111 Rating: (174)
|
Hello Millsite, Which TIA Portal version do you have? Which error message do you receive? Best regards Siwarexi |
9/9/2019 10:44 AM | |
Joined: 1/4/2007 Last visit: 4/18/2024 Posts: 1111 Rating: (174)
|
Hello Millsite, Unfortunately I don’t receive an error message by changing the PLC from CPU315 to CPU319. Attached you can find my TIA Portal project. This project is without the visualisation, because with the visualisation the project would be too large for this Forum. Best regards Siwarexi AttachmentWP321_CPU319_TIA_V15.1.zip (116 Downloads) |
9/9/2019 3:57 PM | |
Joined: 1/4/2007 Last visit: 4/18/2024 Posts: 1111 Rating: (174)
|
Hello Millsite, Attached the required TIA Project. Best regards Siwarexi AttachmentWP321_CPU319_TIA_V15.1_Rev1.zip (155 Downloads) |
Follow us on