2/18/2013 12:52 PM | |
Joined: 1/3/2006 Last visit: 2/19/2024 Posts: 726 Rating: (71) |
Hi Fix a thermostat inside a panel, connect it with AI. You shall get the temperature ! |
2/18/2013 5:46 PM | |
Joined: 1/3/2006 Last visit: 2/19/2024 Posts: 726 Rating: (71) |
Umencho the size of cabin + the calculation of heat dessipation from equiments like drives + fan size installed, determines the size of air conditioner. What if you have fire inside the panel? What if installed air conditioner fails? What if fan fails? There can be many reasons for rise in temperatur inside the panel. And installing thermostats which can provide DI can prove to be very benefecial, I believe. A usefullink.
|
2/18/2013 5:52 PM | |
Posts: 8946 Rating: (999) |
If heaven is falling down, all birds are dead. I NEVER heard, that somebody make an PLC temperature measurement because he was afraid of fire in the cubicle... It sounds a little bit like a joke for me... |
This contribution was helpful to1 thankful Users |
2/18/2013 6:01 PM |
|
Posts: 8946 Rating: (999) |
May be, this link is helpfully: http://www.amazon.com/b?ie=UTF8&node=13400621 |
2/18/2013 6:47 PM |
|
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Please Respect! |
2/19/2013 6:01 PM |
|
Posts: 8946 Rating: (999) |
No, its just intellectual superiority. |
2/19/2013 6:52 PM |
|
Joined: 1/3/2006 Last visit: 2/19/2024 Posts: 726 Rating: (71) |
Oh My God The son of Werner Won Siemens !
|
2/24/2013 8:26 PM | |
Joined: 1/28/2009 Last visit: 5/2/2024 Posts: 6838 Rating: (1359)
|
Dear friends, About the controversial fire detection for panels, I consulted one of my friends (Expert in Fire and Gas) and I came across idea of "EWSD:Early Warning Smoke Detector" .I searched the idea via Google and I found some solution. I share an application for "Data & Telecom" ,I found here.I know, the application would be expensive, but can be applied if necessary. Many regards Hamid Hosseini AttachmentEWSD.pdf (230 Downloads) |
This contribution was helpful to2 thankful Users |
2/28/2013 5:43 PM | |
Posts: 8946 Rating: (999) |
|
This contribution was helpful to1 thankful Users |
Follow us on