4/27/2016 4:44 PM | |
Joined: 5/28/2008 Last visit: 10/12/2024 Posts: 4515 Rating: (839) |
Hello, Did you programmed the letters to appear in its mirror image? If answer is "No", then it's not software problem. As wizard told, perform OS update with reset to factory setting and I hope the KTP will work after that. How do you do an "Operating system update" (OS update) or "Reset to factory settings" on operator panels?If not, then there will be a hardware problem. |
Ayman Elotaify |
|
This contribution was helpful to2 thankful Users |
4/27/2016 4:52 PM | |
Joined: 4/24/2006 Last visit: 10/10/2024 Posts: 8745 Rating: (1168)
|
Hello, When you use WinCC flexible, you can go to option -> Delete temporary files Best regards, Wizard |
4/28/2016 6:08 PM | |
Joined: 3/28/2015 Last visit: 10/4/2024 Posts: 721 Rating: (213) |
Hello, I think the problem due to HW failure in the electronic card of the panel. |
Eng.Mohamed Ibrahim |
|
Follow us on