10/17/2010 10:38 AM | |
Posts: 4 Rating: (0) |
What I have: I am using the logo 7th generation 12/24RC with the digital module,6ED1 0551MB000BA1 12/24R. What I am trying to acheive: I have a double acting air cyclinder with a through rod. One end of the rod has a cup and the other end a clutch plate, the cyclinder is mounted on a 3kg load cell. The sequence is as follows: 1. the rod is fully exteneded, waits for about 15s to fill with flake. 2. the rod retracts inside the unit scrapping the top edge as it goes. 3. stops and weighs. 4. fully retracts, clutch engages, rotates the cup to empty, locates it upright. 5. extends the cup to weigh position and zeros the weight. 6 back to one again to repeat the process. I am learning fast but not fast enough and I need some help on this. I would appreciate any help. I have attached my first attempt at this. Don't laugh please. AttachmentLOGO!Soft Comfort - Density checker 1.pdf (350 Downloads) |
10/18/2010 9:33 AM | |
Posts: 4 Rating: (0) |
Here is my attempt so far all zipped up. Thanks for your help.
AttachmentDensity checker 1.zip (341 Downloads) |
10/18/2010 11:41 AM | |
Posts: 4 Rating: (0) |
I have used the simutation and it works to a point, but I feel there might be an easier way. I cannot get it to recycle. |
Follow us on