12/19/2008 11:42 AM | |
Posts: 6 Rating: (0) |
here's detail of error: the standard devive is indicating 170m3/s, the error device is indicating 178m3/s or 140m3/s |
12/19/2008 11:42 AM | |
Posts: 6 Rating: (0) |
here's detail of error: the standard devive is indicating 170m3/s, the error device is indicating 178m3/s or 140m3/s |
12/19/2008 8:47 PM | |
Joined: 3/29/2007 Last visit: 1/31/2022 Posts: 14 Rating: (2) |
Let me Know. Your installation is new. The error of measure can be produce for bad installation, or bad selection of instrument. If you select the flow meter, do you need use the program "Product Sizing". This program is used for select the correct flow meter, for example the flow meter is select for a minimum flow, all instrument have the minimum scale value with acceptable error (in the Mag 5000 0,5%).The product sizing in the web is https://pia.khe.siemens.com/index_electromagnetic_flowmeters-11382.htm Download https://www.pia-selector.automation.siemens.com/scripts/wgate/zstore3/!?~okcode=EV_INIT-EV_IPC&prod_id=GWK--7MF1003&~template=frameset&~language=EN The installation is very important. The correct flow conditions are vital, for a good function. See page 4/20 to 4/27, of instrument process catalog (Siemens FI 01 · 2009) Catalogs https://pia.khe.siemens.com/index.aspx?Nr=2152 Best Regards Santiago Thomassey Argentina |
Last edited by: ARGThomassey at: 12/19/2008 8:57 PM |
|
12/23/2008 1:55 AM | |
Posts: 6 Rating: (0) |
MAG Flow verificator, what is it? Can you show me? thanks alot |
12/23/2008 10:22 AM | |
Joined: 9/27/2006 Last visit: 3/28/2024 Posts: 12249 Rating: (2660) |
Hello oishi; The Verificator is a hardware/software tool that allows different tests to be done on the Sitrans FM Magflo 5000 and 6000 flowmeters. follow this link to look at some catalog pages describing the tool: http://www.lesman.com/unleashd/catalog/transmit/sitransfm_verificator_cat.pdf Youcan downloadthe Sitrans F MMagflo verificator software from the Siemens support website, here: http://support.automation.siemens.com/WW/view/en/21230153 This FAQ also discusses possible results from the Verificator application: http://support.automation.siemens.com/WW/view/en/21402331 Hope this helps, Daniel Chartier |
Follow us on