12/11/2018 2:23 PM | |
Joined: 7/18/2017 Last visit: 11/15/2023 Posts: 2 Rating: (0) |
Heloo, I have the problem with mag5000,it show triangles with f70 problem,it's also reading negative values and it change the value every moment...from -30 to+30,40 l/m3 ...I try to see in manu settings...but all setings are the same like in the other one...I have three mag5000 in same mesure point...every of them mesure diferent pipe flow...the other one don't have triangles but mesurre is also from - to +....and just third one is working fine...can you tell me what to check? thanks
------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/11/2018 3:07:33 PMNew subject after splitting |
|
Follow us on