12/16/2019 8:46 PM | |
Posts: 200 Rating: (6) |
Hi I would like to control a output Q1 using 1 button I1 I would also like to us the same button to switch of Q1 I have tried this as attached but don't seem to be getting it correct as when the output is active i need it on for 1 hour then when i press agin reset the timer to zero. When i try this it just resets the timer. Thanks Andrew AttachmentCircuit Diagram1.lsc.zip (188 Downloads) |
12/16/2019 8:59 PM | |
Joined: 12/18/2014 Last visit: 9/19/2024 Posts: 33799 Rating: (4199)
|
Something like this with a multiple function Switch? Short press set output with off-delay time. If off-delay time runs and you press short again, the Switch the output off. Press the button longer then 1s, output switch on and stays always on. Again a short press switch off the output. AttachmentCircuit Diagram2.zip (218 Downloads) |
This contribution was helpful to1 thankful Users |
12/16/2019 9:33 PM | |
Posts: 200 Rating: (6) |
Thanks Very much for the reply Its amazing simple it can become Thanks Andrew |
This contribution was helpful to1 thankful Users |
Follow us on