9/25/2007 7:24 AM | |
Posts: 112 Rating: (10) |
This should not be possible unless you have more than one CPU. Post screen shots of hardware setup if you still have problems. |
9/25/2007 8:47 AM | |
Joined: 4/24/2006 Last visit: 4/22/2024 Posts: 8611 Rating: (1147) |
Hi, I think you are using a CP342-5 to use Profibus! In that case it's possible to have those addresses. Here is a link about CP342-5 and how it is used in Project. (differences between CPU and CP342-5) http://support.automation.siemens.com/WW/view/en/18208090 So in the programm you useDP_send and DP_recv to communicate with remote I/O I hope it will help you. Best regards, Wizard |
9/26/2007 1:30 AM | |
Posts: 14 Rating: (0) |
So is there any way (or has anyone come up with a way) to communicate to theperipheral deviceswithout using the DP_SEND and DP_RECV blocks? |
Follow us on