10/21/2009 9:40 AM | |
Joined: 5/28/2008 Last visit: 4/15/2024 Posts: 4505 Rating: (835) |
Dear dezuna, First, welcome to Siemens Automation Family. Second, after downloading the software on the CPU, you can keep connected to the CPU and open the block and monitor it to see why the CPU do not executetheprogram / instructions. Also you can send your program here to let us help you. One other thing, Did you make your instructions in a FC? and did you called this FC in OB1? If not the program won't be executed. To do so, open OB1, and if your program is in FC1 write the following instruction in STL Call FC1 Good luck |
Ayman Elotaify |
|
10/21/2009 12:32 PM | |
Joined: 3/21/2006 Last visit: 4/4/2024 Posts: 10228 Rating: (1181) |
Hello, So, if I understood this is real hardware. I mean, in input I0.0 you connect something (sensor). And when this signal is activate you should receive 'one'. First of all, most important is hardware connection. For this look at http://support.automation.siemens.com/WW/view/en/8859629. Look at attachment. And you also could attach your project. This would be helpful. Regards AttachmentExample.zip (180 Downloads) |
Last edited by: O_Moderator at: 10/21/2009 12:34 PMlink edited |
|
Follow us on