3/6/2009 2:37 PM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating: (1181) |
Hello sharo, Wizard is right. Ask Danfoss for some details. I mean is there have some important points to know when is changing drive from VLT5000 to FC300 regard profibus settings. For the moment Danfoss hasn't example with FC300. Only with VLT2800 drive. I suggest you to look another with VLT5000 (like your old drive). But I thing you don't need this examples. You have already worked with this drive via Profibus. Or no? So try to set all addresses, type of PPO in FC300 like VLT 5000 and download program to the CPU. Only one thing is important. You must set in drive side (mean FC300 drive) the same settings for profibus communication like in VLT5000. Hope this way will works. regards AttachmentVLT5000.zip (699 Downloads) |
Follow us on