2/23/2020 11:59 AM | |
Posts: 11 Rating: (0) |
Hi I have a problem in BMB Machine uses s7-300 Problem is " OUTPUT Addresses are out of range" Any advice... Thanks.. |
2/23/2020 2:11 PM | |
Joined: 12/18/2014 Last visit: 4/26/2024 Posts: 32894 Rating: (4066) |
Please show us the diagnostic buffer. Right click on CPU > PLC > Module Information. Then please upload the saved dignostic file. See attachment. AttachmentScreenshots.zip (114 Downloads) |
This contribution was helpful to1 thankful Users |
2/23/2020 2:33 PM | |
Posts: 11 Rating: (0) |
I can't go online now with this plc There is another way please |
2/23/2020 5:36 PM | |
Posts: 11 Rating: (0) |
Hi sir ; Plc leds operate at normal condition No BF or SF The error during starting of machine appear on HMI Could u tell me the cable for cpu 388-4 And FM 356-4 |
2/23/2020 6:08 PM | |
Joined: 9/27/2006 Last visit: 4/26/2024 Posts: 12257 Rating: (2665)
|
Hello qwertfgn; A CPU 388-4 is an M7 CPU, very different from an S7. It is programmed with Borland C, for example. And M7 units were discontinued around 2002... I, for one, am not competent to help you with this CPU, a side from providing this manual, the only document I found on the CPU 388-4: https://support.industry.siemens.com/cs/ww/en/view/1177102 If no one else on the forum is able to volunteer their help on this machine, I can only suggest you try contacting Siemens Support techs with a Support Request. They may be able to locate someone with experience on a M7 program. The link can be found on the top of this page. There are chapters describing this CPU in the M7 manual, including the requirement for an MPI link for programming. On a modern CPU you would probably look for a PC Adapter USB cable, 6GK1511-0AB00-0AA0. Hope this helps, |
Last edited by: dchartier at: 02/23/2020 18:11:41Last edited by: dchartier at: 02/23/2020 18:12:45 |
|
This contribution was helpful to2 thankful Users |
2/23/2020 7:58 PM | |
Posts: 11 Rating: (0) |
Thanks a lot sir ; Now At starting sd led turns on and after some seconds SF led turns on Is this hardware problem? |
Follow us on