5/25/2018 9:30 AM | |
Posts: 8 Rating:
|
HERE IS MY PUT INSTRUCTION AND DIALOG SETTING |
5/25/2018 10:12 AM | |
Posts: 8 Rating:
|
i've checked the Status and Error Parameter when the req is true, the error sends bit low (zero) when the req is false, the error sends bit high (one), and the status is 0001 in HEX, then change to 0019 hex it means 25 in decimal, i've read the description about the error = 1 and status = 25 im sure my connection is uninterrupted and in run mode and also ive checked the memory area at the partner cpu it gives 0000 value in hex AttachmentSTATUS AND ERROR PARAMETER.avi (519 Downloads) |
5/25/2018 10:13 AM | |
Posts: 8 Rating:
|
and this pic is about memory area on the partner cpu output |
5/25/2018 10:26 AM | |
Posts: 8 Rating:
|
im using one second timer pulse input to the req, if i wrong, what should i use to fill the req input ? |
Follow us on