1/17/2020 8:45 AM | |
Joined: 12/27/2018 Last visit: 9/18/2024 Posts: 510 Rating: (43) |
Please see the link below |
Jinson James, M.Tech (Power Electronics and Power System), |
|
1/29/2020 10:21 AM | |
Joined: 8/3/2009 Last visit: 9/18/2024 Posts: 13728 Rating: (1728)
|
Hello gesteen the only Solution that is available for this is in this FAQ, but you already know, and you also have written that you cannot use the S71500 for this in your special usecase: https://support.industry.siemens.com/cs/de/en/view/109482675 An easy automatical way in the Comfort Panels is not possible! Of course you can use the Scheduled Tasks with an every day Task and a Script that reads out the current date and then you have to calculate or yourself if the Summertime is active or not (and then use the Systemfunction for activating the Summertime or deactivate) But its not that easy to calculate it. Bye Murof |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to1 thankful Users |
Follow us on