3/17/2016 10:16 AM | |
Posts: 25 Rating: (0) |
Hey guys, I have recieved a LOGO! from my work to hobby with, but I got connection problems with it. I can read from the LOGO! but I can't download software in it. When I do i get an error which says ''transmission error'' (COM17 port is not available'') The COM 16 port is the only one I can select in the interface window. I've already configured my LOGO! to the right version which is: 0ED1 - 0531 - 1BB00 - 0BA2. >> Configured as 0BA2 standard in LOGO! soft comfort V7.0 The cable i use is a LOGO cable with at the end a D - sub 9 pin connector. The D - sub connector is placed in the Serial usb > dsub converter.and then ofcourse in my laptop ACER - aspire V3571G Hopefully someone can help me further. Thanks in advance. |
3/17/2016 10:17 AM | |
Posts: 25 Rating: (0) |
Picture 2 |
3/17/2016 10:18 AM | |
Posts: 25 Rating: (0) |
Picture 3.. |
3/17/2016 10:25 AM | |
Joined: 12/18/2014 Last visit: 5/14/2024 Posts: 33027 Rating: (4082) |
Take a look at this Topic: |
3/17/2016 3:06 PM | |
Posts: 25 Rating: (0) |
Downloading LSC 8 isn't for me an option. I'm sorry, but that topic can't help me further. |
Last edited by: monis71 at: 3/17/2016 3:07:37 PM |
|
3/17/2016 3:26 PM | |
Joined: 12/18/2014 Last visit: 5/14/2024 Posts: 33027 Rating: (4082) |
Why not? |
3/17/2016 4:07 PM | |
Posts: 25 Rating: (0) |
I don't want to pay 60 euro's for a program that ''may'' fix my issue. |
3/17/2016 4:09 PM | |||||||||||||||||||||||||||||||||||||
Posts: 25 Rating: (0) |
Thanks for pointing that out! however, i've already tried this and this didn't solve the issue. I still get the transmission error :( |
||||||||||||||||||||||||||||||||||||
Last edited by: monis71 at: 3/17/2016 4:10:26 PMLast edited by: monis71 at: 3/17/2016 4:12:11 PM |
|||||||||||||||||||||||||||||||||||||
3/17/2016 4:27 PM | |
Joined: 12/18/2014 Last visit: 5/14/2024 Posts: 33027 Rating: (4082) |
If you have a fullversion of a older LSC Version, you can upgrade LSC for free. Open LSC, then in the menubar: help > update-Center. Follow the steps. |
Follow us on