2/18/2010 8:34 AM | |
Joined: 9/7/2009 Last visit: 3/6/2024 Posts: 1 Rating: (0) |
To the Expert kindly help me. Our system was working with current transmitter (Brand : WEIGEL A1U 2.2), 4-20mA and 4 wire configuration. Analog Input Module is 331-7KF02-0AB0. When one of the transducer was found defective, we replace and then by thistimewe encounter that the HMI scree will directly display the maximum range even in stop mode. I try to measure using mA meter, reading is 4.00 mA. We already try all the spare unit but the same thing was happen. AttachmentCurrent_transducerA1U2.2_e.pdf (180 Downloads) |
Follow us on