8/3/2017 3:36 AM | |
Joined: 7/1/2011 Last visit: 3/21/2024 Posts: 2 Rating: (0) |
I am getting zero reading at the display on client WINCC Scada. The Siwarex module I am using is 7MH4950-1AA01, When I check the voltage Sense+ sense - = 6V EXC+ EXC - = 6V SIG+ SIG - = 1.8mV When I check the Siwarex module LED's SF is ON ST1 OFF ST2 is ON load cell is connected as channel 1, I am using SFC58 and SFC59, to rad and write When I check in the PLC
can anybody help me why I am not getting the Gross weight value? how I can rectify this issue.? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 8/3/2017 1:58:58 PMNew subject after splitting |
|
Follow us on