12/10/2008 4:55 PM | |
Joined: 12/10/2008 Last visit: 1/8/2009 Posts: 3 Rating: (0) |
What is the status and/or timeline on the compatibility issue ? |
12/10/2008 5:30 PM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating: (1181) |
Hello SW Prerequisites:Windows XP SP2 ,Windows XP embedded Image of the SIMATIC PCs regards |
12/12/2008 12:47 AM | |
Joined: 5/19/2007 Last visit: 12/23/2023 Posts: 14 Rating: (0) |
|
1/7/2009 2:46 PM | |
Joined: 11/15/2006 Last visit: 5/7/2021 Posts: 1319 Rating: (172) |
SP1 for WinAC RTX 2008 has been released which is now released for XP SP3: http://support.automation.siemens.com/WW/view/en/33563717 |
Have Fun! |
|
2/20/2009 12:32 PM | |
Posts: 7 Rating: (0) |
How do you install RTX2008 on Windows SP3? - I tryed to install WinAC RTX 2008 (no SP1) on a windows SP3. ==>>the installationisn't possible on SP3, Windows SP2 is needed - I downloadedWinAC_RTX_2008_SP1.exeand execute it. ==>> No installation possible, installation of SIMATIC Windows Logic Controller RTX v4.4needed. - In SIMATIC WinAC RTX 2008 Service Pack 1 Released,i can read this: Installation of IntervalZero RTX V8.1 SP1To be able to run WinAC RTX 2008 under Windows XP Professional with SP3 it is necessary to install Service Pack1 for the IntervalZero RTX V8.1 realtime core (previously: Ardence RTX) which is used by WinAC RTX. The Service Pack can be downloaded from the following link ...For installation please proceed as follows:
Marvellous, i concluded it's impossible to install RTX 2008without windows SP2. If my OS is a windows SP3, no solution is given. |