12/26/2019 11:27 AM | |
Joined: 9/23/2005 Last visit: 4/17/2024 Posts: 4325 Rating: (1424) |
Hi, “Simple Samples” are small projects that demonstrate simple features. The target is giving a quick overview about the theme and be used as start point for related discussions. Follow there are a short description and the configuration main steps. Trends are an important tool for process signals evaluation. There is many variations about trends and trends object settings. Here there is two variants of then: real time variable trends and data log trends. Configuration main steps:
TIP: To add more tags to the Trend Object, go to General → Trend Areas → [0] Trend Area → Trends; Click on 1 Object, "..." button, <Add new> TIP: To split the Trend Area in separet trends, go to General → Trend Areas; Click on 1 Object, "..." button, <Add new>
Additional step for the second variante (Data Log Trends)
TIPs:
Project (.zap16 ziped as .zip)
AttachmentTrends.zip (1094 Downloads) |
Last edited by: Denilson Pegaia at: 12/30/2019 18:49:08Last edited by: Denilson Pegaia at: 01/23/2021 20:27:02Last edited by: Denilson Pegaia at: 02/03/2021 10:55:00Denilson Pegaia |
|
This contribution was helpful to5 thankful Users |
10/11/2022 5:24 PM | |
Joined: 9/23/2005 Last visit: 4/17/2024 Posts: 4325 Rating: (1424)
|
Hi The control object Process Control could also be used to show the trends in a table format. Se example attached AttachmentTrends_V17_20221011_1403.zip (588 Downloads) |
Denilson Pegaia |
|
12/27/2023 10:38 AM | |
Joined: 9/23/2005 Last visit: 4/17/2024 Posts: 4325 Rating: (1424)
|
Hi As from TIA V19, there are simplified views for Alarm Control & Trend Control. The simplified design improves the handling of screen space utilization. TIPs:
Sample project (archived from TIA Portal as .zap19 and after that compacted in .zip format to be uploaded here) user= User, all password = Password1! Attachmentalarm trend.zip (182 Downloads) |
Denilson Pegaia |
|
This contribution was helpful to1 thankful Users |
Follow us on