6/10/2013 4:31 PM | |
Posts: 58 Rating: (0) |
Hello Can anybody help me? I have the next doubt with a configuration of the WP231 module, i havea load cell with the next characteristics: four wires,Range 0-100 N (Newtons), the output is 1mv/V, but my problem is that the configuration in siwatool is not clearly, i put a load and it has a lot of difference when i put it again and again, and the zero is not automatic i always have a measure without load. It suppose that the parameters are referenced to kilograms so i put 10.2Kg the Nominal load cell cause is up to 100N, i connect four wires as a six wires i attached the wiring diagram. And also i attached the Final calibration of the load cell. With this calibration can i configure directly the wp231 to get the output in Newtons cause i have the calibration as 100Newtons = 3.775 mVdc = 3.815 Normalized Data Or is only with kilograms? Can you help me with your opinion about configuring this load cell Thanks a lot AttachmentWP231 CONFIG.zip (349 Downloads) |
Last edited by: O_Moderator at: 6/11/2013 8:31 AM |
|
6/10/2013 5:24 PM | |
Joined: 7/7/2010 Last visit: 5/10/2024 Posts: 14709 Rating: (2356)
|
This quick start guide may help in case you had not already seen it: https://support.automation.siemens.com/WW/llisapi.dll/csfetch/73517989/SIWAREX_WP231_Quick_Guide_SIWATOOL_V1_5.pdf?func=cslib.csFetch&nodeid=73516531&forcedownload=true |
science guy |
|
7/11/2014 1:23 PM | |
Joined: 3/25/2013 Last visit: 3/21/2019 Posts: 176 Rating: (1) |
New question split intohow to configurate siwarex function block8 on tia portal v11 sp2 up5. With best regards, Narrator1
|
Follow us on