8/28/2014 2:18 PM | |
Joined: 1/4/2007 Last visit: 4/18/2024 Posts: 1111 Rating: (174)
|
Hello subin, The weight value is not updated faster. The update of a new value is the same. The updating of the weight value is independent of the low pass filter. The difference by using different values for the low pass filter is the “step function response”. That means if you put suddenly a load on the load cell, then the time until you see the correct new weight value is faster (by using the low pass filter settings “1”, “2” or “5”) or the time until you see the correct new weight value is more slowly(by using the low pass filter settings “0.2”, “0.1”). I found a FAQ on the internet for the Siwarex FTA module. This FAQ is also valid for the WP231. Maybe this FAQ helps you: http://support.automation.siemens.com/WW/view/en/30577386 Into that FAQ you can see the setting “filter: 1Hz” and “filter: 0.1Hz”: By using the 0.1Hz you can see that the time is longer to show the new weight value. Best regards Siwarexi |
2/2/2015 11:45 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4774 Rating: (123) |
|
Follow us on