3/20/2015 4:22 AM | |
Posts: 2 Rating:
|
Dear Mr.
I used to cpu1214 with CM1241 RS485 communication with the SOCOMEC DIRIS A20 (Modbus RTU), but an error occurred 8383, I have tried many ways but still no success. In the attached file is the project that I've done and error code. You see there is a program to send to help me. Thank you
----------------------------------------------------------------------------------------------------
AttachmentComm_S1200_Socomec A20_V13.rar (229 Downloads) |
Last edited by: Min_Moderator at: 3/20/2015 9:40:02 AMNew subject after splitting |
|
3/20/2015 2:17 PM | |
Posts: 1058 Rating:
|
hello expert123456, your problem has already been discussed here: Error Code 8383 | S7-1200 | Modbus RTU Slave CM1241 RS485 Modbus RTU Allowed Code S7-1200 - Modbus RTU comms with third party slave S71200 Modbus TCP Communication with SOCOMEC DIRIS A40
You will find a sample program for Modbus TCP communication here: Sample Program: Modbus TCP with S7-1500
regards
|
Follow us on