2/12/2016 11:30 PM | |
Joined: 9/27/2006 Last visit: 9/10/2024 Posts: 12282 Rating:
|
Hello HP; The following document and software download might be helpful, to setup yur IO-Link bus:
https://support.industry.siemens.com/cs/ww/en/view/65949252 IO-Link configuration tool Configuration tools are required to configure the entire IO-Link system. The IO-Link configuration tools of the master manufacturers are able to read IODDs. The main tasks of the IO-Link configuration tool include: ● Assigning the devices to the ports of the master ● Address assignment of ports within the address area of the master ● Assigning parameters for the IO-Link device Diagnostics can also be carried out on the connected devices. This means the IO-Link configuration tool supports the transparent representation of the IO-Link system down to field level. Siemens
provides S7-PCT for engineering of the IO-Link system.
https://support.industry.siemens.com/cs/ww/en/view/32469496 Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 2/12/2016 11:32:20 PM |
|
Follow us on