5/2/2016 9:52 AM | |
Posts: 7 Rating: (1) |
Hi, I want to read two 16 bit float modbus address as single 32-bit float value in Wincc Runtime SCADA (TIA Portal V13). Anyone tel me either VB Script or Internal Instruction to SWAP the these data without using PLC. I used formula As you said above I used two 40001 & 40002 tags as Float data type and Real Value tag as Real data type. When i go online simulation i got ( ######) symbol in I/O field. Could any one please tel me what is the procedure and solutions. Thank you. ------------------------------------------------------------------------------------------ |
Last edited by: JairaJ at: 5/2/2016 10:01:11 AMLast edited by: JairaJ at: 5/2/2016 11:23:58 AMLast edited by: JairaJ at: 5/2/2016 11:25:18 AMLast edited by: Blue Moderator at: 5/2/2016 12:43:19 PMNew subject after splitting |
|
Follow us on