6/7/2016 8:18 AM | |
Joined: 1/27/2015 Last visit: 1/24/2024 Posts: 53 Rating:
|
Hello dan90, is there are a 'built in' Modbus communication functionallity in the panels? Or do you use Modbus blocks in PLC for communication which are controlled over the panel? What device is 'the other side'? Does it happen only one time or comes this error again? Because you wrote you copied from an other project and than it works? Regards bachgeist |
Follow us on