7/4/2017 7:15 AM | |
Posts: 6 Rating:
|
Hi We have an application which is in Linux PC and we want to communicate with S7 1200 through open TCP socket program. Currently, if we have to communicate with only one socket connection, then it is only able to read or write and not both in the same socket . Is there any restriction like that, can we create different port numbers of sorts to read and receive in the same socket ? Thanks, Ram ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 7/4/2017 1:42:29 PMNew subject after splitting |
|
Follow us on