12/6/2018 4:16 PM | |
Joined: 9/27/2006 Last visit: 6/16/2024 Posts: 12260 Rating:
|
Hello minh_nq; After looking at the documents in the Berthold site on the LB 452 and the various sensors it can connect to, there seems to be very little information on the data exchanges inside the system. The sensors seem to transmit pulsed signals to the LB 452 controller, and it uses its internal software to extract information that can be later sent to a Profibus master (see the gsd file for the LB 452 for more details on the Profibus communications).. https://www.berthold.com/en/pc/level-measurement/mold-level-measurement/castxpert-lb-452 I do not think it is possible to connect a sensor directly to a PLC communication card, unless you have a lot more information on what the transmissions actually mean... There is contact information for sales and support on the webpage proposed above, you could reach out to Berthold personnel and enquire directly to them on your options. Hope thois helps, Daniel Chartier |
This contribution was helpful to
2 thankful Users |
Follow us on