2/3/2011 2:16 AM | |
Joined: 9/27/2006 Last visit: 6/16/2024 Posts: 12260 Rating:
|
Hello MGP; The Siplus RIC bundles for IEC 60870-5-104 would be your best bet, in Siemens' world. The last post in this (rather dated) thread mentions links to S7-400H libraries for the Siplus RIC, so hopefully they have evolved since then. /tf/WW/en/Posts/19771 The thread also mentions alternative offers of OPC gateways that you could look at. Hope this helps, Daniel Chartier |
2/5/2011 9:52 PM | |
Joined: 9/27/2006 Last visit: 6/16/2024 Posts: 12260 Rating:
|
Hello MGP; The Siplus RIC systems are not licenses, but "bundles" that include hardware (S7-300[or other]CPUs, MMC and communication processors) and software drivers that allow connection to IEC protocols. Have a look here for more descriptions: https://www.automation.siemens.com/mcms/topics/en/siplus/ric-telecontrol/bundle-s7-300/Pages/default.aspx Use the links on the right of the page to locate system descriptions and technical information. For a introduction manual to the software driver (IeConS7), dowload the pdf at this link: http://www.automatyka.siemens.pl/docs/docs_as/IEConS7_manual_V1_2.pdf Last but not least, Mr, G, Sucher offers to help you out with information oin these systems (he is part of the development team, it seems) as you have seen in the link provided earlier. So take advantage of it and PM him. Hope this helps, Daniel Chartier |
This contribution was helpful to
1 thankful Users |
Follow us on