8/30/2011 3:06 PM | |
Posts: 13 Rating: (0) |
I have a complete and industrial example that control vacon drive via profibus.I am not Professional in stl. can anyone explain this program to me. i attach the program http://www.vacon.com/File.aspx?id=455773&ext=pdf&routing=396771&name=Ud188G please help me AttachmentVacon.zip (605 Downloads) |
Last edited by: chelina2 at: 8/30/2011 3:09 PM |
|
8/30/2011 5:54 PM | |
Joined: 4/22/2010 Last visit: 5/3/2024 Posts: 5697 Rating: (714) |
Hello, Not mutch happening in that FB, just a few move's from the inputs of the FB to the outputs off the FB, some calculations for speed torque, etc and some conversions to get the bits at the right format and place. I think (let us know if i'm wrong) you want to know how to use this block) Well, start with deleting the DB 22, then open OB1 in ladder or FBD. Call FB22 and let Step-7 generate a new DB22. Now you can see the Block with inputs and outputs (with comment) You have to get a GSD file to import in your hardware config, to let this FB work. Attached the program, with the changes. If you need to know more, let us know. Regards, Marcjan AttachmentVacon__1.zip (460 Downloads) |
Last edited by: Marcjan at: 8/31/2011 9:09 AMLast edited by: Marcjan at: 8/30/2011 5:56 PMto mutch typo''''''''s :-( Problem solved? |
|
9/1/2011 4:16 PM | |
Posts: 13 Rating: (0) |
thanks for your attention Dear Marcjan i im working with cemat(blockes) in pcs7 and i want to create functiion to comunicate with several sets such as schenk(weight feeder) or PDRIVE or VACON drive, abb relayes and so on via profibus. i want to create these blockes and i have several industrial examples in S7 but i cannot understand this programs that is difficult to me. actully i want anyone who can understand this programs and instructions and procedure of sending and reciving data from profibus, explane program to me untel i able to write this program ownly. for example i cannot understand in network 1 why input address of hardware begin is shift left??? slw3 and then Lar1 and.... i try very lot to understand this programs but i... please help me |
9/1/2011 5:33 PM | |
Joined: 4/22/2010 Last visit: 5/3/2024 Posts: 5697 Rating: (714) |
O.k., now whe know why you want the explanation off that block. I have at the moment no acces to my S7 tools, can have a look at it next day. But there are others here, real cracks so don't worry. Have attached a explanation off all the STL commands, hope that helps you a bit. Regards, Marcjan AttachmentSTL-cheat-sheet-by-category.pdf (483 Downloads) |
Problem solved? |
|
9/3/2011 7:13 AM | |
Posts: 13 Rating: (0) |
thanks Dear Marcan Already i have read : https://support.automation.siemens.com/WW/llisapi.dll?func=cslib.csinfo&objId=24519683&nodeid0=10805384&load=content&lang=en&siteid=cseus&aktprim=0&objaction=csview&extranet=standard&viewreg=WW that was useful but cannot help me to understand program. first we ought know PPO(Parameter/Process Data Object) in vacon profibus manual and then write S7 program. i know we recieve several data such as Ready or Fualt and so on via profibus throw "Status Word"(in page 28 of attached manual)and send speed set point via "Control Word"(in page 27) But i cannot understand properly how my sent S7 program does this task please illustrate to me how does it AttachmentVacon_Profibus_english_UD00711I.pdf (599 Downloads) |
9/5/2011 2:07 PM | |
Posts: 13 Rating: (0) |
Isnt here anyone to help me? |
9/5/2011 3:04 PM | |
Joined: 4/22/2010 Last visit: 5/3/2024 Posts: 5697 Rating: (714) |
Hello, I have put some comments in your FB, see attachment. Running out off time so not all networks done yet. Hope this helps. Regards, Marcjan AttachmentFB22.pdf (529 Downloads) |
Problem solved? |
|
9/6/2011 9:48 AM | |
Posts: 13 Rating: (0) |
Dear Marcan thanks very very very lot |
This contribution was helpful to1 thankful Users |
9/6/2011 12:42 PM | |
Posts: 13 Rating: (0) |
hello can we use LAR1 P## AdressI instead of: L #AdressI SLW 3 LAR1 that is true? |
7/19/2018 10:44 AM | |
Joined: 6/19/2017 Last visit: 5/31/2024 Posts: 8110 Rating: (165) |
New question published by AutoGen_7146170 is split to a separate thread with the subject Trying to implement this block on step 7, 5.6 , vacon20 and the opte5 card. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on