5/30/2012 10:29 AM | |
Joined: 3/2/2012 Last visit: 5/23/2013 Posts: 5 Rating:
|
Hello sprawl, Thank you for reply.. What you have mentioned, we have done that before. Yes.. TC_CON is working.. but at thetime of sending( PLC to Mobile) only.. In TC_RECV block, Busy just toggles. Do we need any specific format of text-body to receive messages from mobile to PLC? I have attached snapshots of program. Please take a look at it and tell me if there are any errors Do you have any sample program? If you have it, thenCan you send me the program? AttachmentSMS snapshots.pdf (980 Downloads) |
6/9/2012 9:01 AM | |
Joined: 3/2/2012 Last visit: 5/23/2013 Posts: 5 Rating:
|
Hello sprawl, Few days ago, my program was working with sending and receiving. But then it stopped working. I checked your post to this thread. --> S7-1200 , CP1242-7 , receive SMS without TELESERVIS You mentioned that an empty sms might cause CP not to receive any messages. Do you think that can be the issue with our case? The problem is, messages get received in SIM card but are not displayed on Receive DB. I checked all those messages when I inserted my SIM card in mobile. All messages were there. There were another problems. 1) When i was able to receive messages, the first two characters of sms were always getting clipped. 2) At the time of sending, PLC adds one special character before each message. Please help me with this. Best Regards, blackstarsoul P.S. I have attached my program with this post. Plz tell me if there is any problem with code. AttachmentSMS.zip (592 Downloads) |
7/6/2012 6:48 AM | |
Posts: 1 Rating:
|
Hello blackstarsoul, you able to receive SMS with the CP1242-7? that you had problems? is that I have your same problem and I can not resolve thanks, ![]() |
Follow us on