9/25/2019 7:38 AM | |
Joined: 4/14/2017 Last visit: 8/2/2023 Posts: 32 Rating: (0) |
Dear All, I have ABB VFD ACS550 with RETA 02 CARD, its communicating through S71500 over profinet. Its getting on off command and giving feed back to plc. The only problems is that VFD is not following the speed ref from plc. I can see the value given from plc as speed ref on vfd panel but vfd not following this reference. when I start vfd locally then its run ok but from remotely its not following speed reference given. ------------------------------------------------------------------------------------------ Attachmentpicss.zip (61 Downloads) |
Last edited by: The Helping Hand at: 09/25/2019 10:08:10New subject after splitting Last edited by: The Helping Hand at: 09/25/2019 10:33:46Added attachment from double post. |
|
This contribution was helpful to1 thankful Users |
Follow us on