11/28/2006 4:56 PM | |
Posts: 5822 Rating: (412)
|
Dear Slartibartfast, I am sorry, but as far as I know is the DF 1 Protocol only released for Point to Point interfaces, e.g. RS 232, TTY or X.27 (RS 422). These physics are not capable of handling multipoint communication. I am fear you have to find another solution for this. Is it not possible to use e.g. a SST PROFIBUS Scanner on AB side? Like in here: Communication between SIMATIC S7-CPUs on PROFIBUS and Allen-Bradley Controllers via SST PROFIBUS Scanner Best regards J_Bell |
2/27/2007 11:04 AM | |
Posts: 13 Rating: (0) |
Is ther also something possible on siemens side because the data highway cable is already in my cabinet Koen |
Follow us on